Hi,
I have a requirement where two processes needs to be created(each runs on encoding use case). Could you please provide me the following information
1. Is DCE multiinstantiable (can dce_init be done multiple times)
2. If not can I call dce_init() in one process and use the same handle in another process to create the encoding instances
3. If (2) is possible how thread/process safe it is to concurrently access the dce from two different processes?
Thank you inadvance
Regards,
Mahi