This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Error: L6218E: Undefined symbol UARTFlushRx and UARTFlushTx (referred from uart_echo.o).

Hi,

I am using UARTFlushTx and UARTFlushRx function in my code, even though if i include the file 'uartstdio.h' can anybody can help?

 

Regards

Bharath MR

  • Bharath,

               These functions are not defined in StarterWare. Have you defined these functions in your code. Why do you want to call these functions.

    Can you please explain more about your build/debug enviromvment.

    Regards

    Baskaran

    Note: If this post answers your question, please click the Verify Answer button below. Thank you!

  • In reply to Baskaran Chidambaram:

    hi,

    thanks for the reply.

    i want to flush Rx and Tx buffer hence i want to use these functions and these fuctions are defined in the uartstdio.h and uartstdio.c

    regards

    Bharath MR

  • In reply to Bharath MR:

    i couldnt find these definitions in uartstdio.c/h.

    Can you send your copy of uartstdio.c..?

    Which SoC are you using AM1808 or AM335x.?

    which compiler are you working on..?

    Note: If this post answers your question, please click the Verify Answer button below. Thank you!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.