• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » StarterWare » StarterWare forum » AM335xEVM example project won’t build and run in CCSv5 with TMS470 compiler
Share
StarterWare
  • Forum
Options
  • Subscribe via RSS

Forums

AM335xEVM example project won’t build and run in CCSv5 with TMS470 compiler

This question is answered
MWagner
Posted by MWagner
on Apr 18 2012 16:15 PM
Prodigy170 points

I’m using CCSv5 (version 5.1.0.09000) with the TMS470 compiler and I can’t get a simple project (eg. buzzerBeep) to build and run with on the EVM board with a Blackhawk USB560 JTAG emulator. I installed the tools on my Windows 7 64-bit machine using the SPRC932A install DVD.

 I can successfully import and compile the buzzerBeep project as shown below, but there are errors with the post-build, namely because no directory tiobj2bin was installed by the DVD installer in the utils. Therefore there is no tiojb2bin.bat or mkhex4bin.exe on my hard drive.

 Then I unsuccessfully tried to load the buzzerBeep.out into the debugger. Is the problem due to these missing utilities? If so, how can I get these missing files installed?

 

**** Build of configuration Debug for project buzzerBeep ****

 C:\ti\ccsv5\utils\bin\gmake -k all

'Building file: C:/ti/AM335X_StarterWare_02_00_00_05/examples/evmAM335x/audio_buzzer/buzzerBeep.c'

'Invoking: TMS470 Compiler'

"C:/ti/ccsv5/tools/compiler/tms470/bin/cl470" -mv7A8 -g --include_path="C:/ti/ccsv5/tools/compiler/tms470/include" --include_path="../../../../../../../include" --include_path="../../../../../../../include/hw" --include_path="../../../../../../../include/armv7a/am335x" --diag_warning=225 -me --abi=eabi --code_state=32 --preproc_with_compile --preproc_dependency="buzzerBeep.pp"  "C:/ti/AM335X_StarterWare_02_00_00_05/examples/evmAM335x/audio_buzzer/buzzerBeep.c"

'Finished building: C:/ti/AM335X_StarterWare_02_00_00_05/examples/evmAM335x/audio_buzzer/buzzerBeep.c'

' '

'Building target: ../../../../../../../binary/armv7a/cgttms470_ccs/am335x/evmAM335x/audio_buzzer/buzzerBeep.out'

'Invoking: TMS470 Linker'

"C:/ti/ccsv5/tools/compiler/tms470/bin/cl470" -mv7A8 -g --diag_warning=225 -me --abi=eabi --code_state=32 -z -m"buzzerBeep.map" --warn_sections -i"C:/ti/ccsv5/tools/compiler/tms470/lib" -i"C:/ti/ccsv5/tools/compiler/tms470/include" --reread_libs --ram_model -o "../../../../../../../binary/armv7a/cgttms470_ccs/am335x/evmAM335x/audio_buzzer/buzzerBeep.out"  "./buzzerBeep.obj" -l"libc.a" -l../buzzerBeep.cmd

<Linking>

'Finished building target: ../../../../../../../binary/armv7a/cgttms470_ccs/am335x/evmAM335x/audio_buzzer/buzzerBeep.out'

' '

C:/ti/ccsv5/utils/bin/gmake --no-print-directory post-build

"C:/ti/ccsv5/utils/tiobj2bin/tiobj2bin.bat"  "../../../../../../../binary/armv7a/cgttms470_ccs/am335x/evmAM335x/audio_buzzer/buzzerBeep.out"  "../../../../../../../binary/armv7a/cgttms470_ccs/am335x/evmAM335x/audio_buzzer/buzzerBeep.bin"  "C:/ti/ccsv5/tools/compiler/tms470/bin/ofd470.exe"  "C:/ti/ccsv5/tools/compiler/tms470/bin/hex470.exe"  "C:/ti/ccsv5/utils/tiobj2bin/mkhex4bin.exe"

The system cannot find the path specified.

gmake[1]: [post-build] Error 1 (ignored)

' '

 **** Build Finished ****

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • MWagner
    Posted by MWagner
    on May 09 2012 13:43 PM
    Prodigy170 points

    I tried a different EVM board with the same Blackhawk debugger, and now everything is functioning properly.

    I still don't understand why the original EVM board works just fine if I run the app from an SD card, copying it into DDR memory. and executing it from there.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • JayWhy
    Posted by JayWhy
    on May 09 2012 14:28 PM
    Intellectual330 points

    How are the EVM boards different? Do they have different profile settings? 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Baskaran Chidambaram
    Posted by Baskaran Chidambaram
    on May 10 2012 01:55 AM
    Expert4385 points

    in the problematic evm,

    Can you take the dump of EMIF registers (0x4C00_0000) and compare them in the following 2 scenarios.

        1. boot the application with bootloader -> connect target with CCS -> get register dump

        2. Conmnect target with CCS -> load gel file -> get register dump

    Regards

    Baskaran

    StarterWare
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • JayWhy
    Posted by JayWhy
    on May 10 2012 12:09 PM
    Verified Answer
    Verified by MWagner
    Intellectual330 points

    I did as Baskaran asked, and found that there are indeed differences. I changed the GEL file to match the register settings from the bootloader, and I am now able to debug applications stored in external DDR. The settings I changed in the GEL file were for DDR termination and DDR_PHY read latency.

    Original GEL file values:

    (line 802) #define OPP100_DDR2_READ_LATENCY 0x04 //CL=4 Max=(CL+7)-1 ie.11-1=10 Min=(CL+1)-1 ie.5-1=4
    (line 807) #define OPP100_DDR2_SDRAM_CONFIG 0x40805332 //no ODT on DDR2 side

    New GEL file values:

    (line 802) #define OPP100_DDR2_READ_LATENCY 0x05 //CL=4 Max=(CL+7)-1 ie.11-1=10 Min=(CL+1)-1 ie.5-1=4
    (line 807) #define OPP100_DDR2_SDRAM_CONFIG 0x43805332 //no ODT on DDR2 side 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • MWagner
    Posted by MWagner
    on May 10 2012 12:30 PM
    Prodigy170 points

    I made the same GEL file DDR setting changes that JayWhy suggested and now I can successfully use the debugger with both EVM boards.

    This is awesome!

    Thanks for you help.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Baskaran Chidambaram
    Posted by Baskaran Chidambaram
    on May 12 2012 01:19 AM
    Expert4385 points

    Wanger, Jay,

             Thanks for the update. Can you share the updated gel file, so that we can evaluate and if needed include the changes in the next release.

    Regards

    Baskaran

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • JayWhy
    Posted by JayWhy
    on May 14 2012 06:33 AM
    Intellectual330 points
    AM335x.gel

    3644.AM335x.gel

    See attached. 

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Alexis Patenaude
    Posted by Alexis Patenaude
    on Jun 04 2012 13:50 PM
    Prodigy20 points

    Hi!

    I had a similar behavior while step-debugging. I found that at one point, the T bit of the CPSR register was switched to 1 when the initial task of the OS is called. This causes the CPU to interpret the ARM instructions in Thumb. Since this doesn't make sense, the PC quickly jumps to unmapped memory locations and finally ends up at  0002008c:   EAFFFFFE B               0x2008C.

    I haven't been able to explain why the T bit of CPSR is set un the first place but I suspect that it requires Supervisor privileges to do the context switch and the CPU is already in user mode at this point.

    Would anynone know how to prevent the CPU to go in User Mode in the _c_int0 boot code? I would like to stay in supervisor until my OS has started.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • eugenio
    Posted by eugenio
    on Oct 03 2012 08:05 AM
    Intellectual560 points

    Same issue. Hardware and toolchain:

    • Cpu AM3359 
    • ICE demoboard rev. 1.0A;
    • am335x_sysbios_ind_sdk_1.0.0.4
    • Code Composer Studio Version: 5.2.0.00069
    After starting debugger and connecting to cpu, bit T of CPSR is set... 
    Maybe something is wrong in debugger launch script.
    I've alwayas experienced this kind of problem (am335x_sysbios_ind_sdk_1.0.0.3 and later), and I overcome that retrying/resetting/restarting the debugger a couple of times before getting it working.

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
12
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use