Hello,
I'm trying to run StarterWare UART example on OMAP-L138 Experimenter Kit.
* Compiling
+ able to compile using GCC
+ NOT able to compile using CCSv5 (the only version CCS can be used, not earlier version)
* Flashing
+ Able to convert to AIS file from GCC OUT file
+ Able to do flashing on to the board correctly.
* PROBLEM
+ Not working. There's nothing on the terminal, no UART echo, ...
* Issues
+ Able to run UART example from the package "CCSv4-2_with_SOM-M1_BSL_WS" under CCS-v4. So nothing wrong with the board and PC termianl
+ Able to get it boot and run example "OMAPL138-DSP-LED" using the flashing procedure above, including AISgen from OUT file, and using CCS-v4. So nothing wrong with AISgen and flashing procedure.
I'd appreciate any help to find out why StarterWare UART not working for me
Thanks,
~Duy-Ky