Hello,
I installed the C6748 StarterWare package at the default location, opened CCS v5.1, and then selected Project -> Import Existing CCS/CCE Eclipse Project. I then traversed down to:
C:\Program Files (x86)\Texas Instruments\C6748_StarterWare_1_20_01_01\build\c674x\cgt_ccs\c6748\evmC6748\mcasp\
to locate the example project file.
When I attempt to build the project, I get the following Warning in the Problem view:
Invalid project path: Include path not found (C:\Program Files (x86)\Texas Instruments\C6748_StarterWare_1_20_01_01\ipclite\include).
In the Console window it shows:
**** Build of configuration Debug for project mcasp_c674x_c6748_evmC6748 ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building file: C:/Program Files (x86)/Texas Instruments/C6748_StarterWare_1_20_01_01/examples/evmC6748/mcasp/aic31.c'
'Invoking: C6000 Compiler'
"C:/ti/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6740 -g --define=c6748 --include_path="C:/ti/ccsv5/tools/compiler/c6000/include" --include_path="../../../../../../../examples/evmC6748/mcasp" --include_path="../../../../../../../include" --include_path="../../../../../../../include/hw" --include_path="../../../../../../../include/c674x" --include_path="../../../../../../../include/c674x/c6748" --include_path="../../../../../../../grlib/include" --include_path="../../../../../../../usblib/include" --include_path="../../../../../../../ipclite/include" --include_path="../../../../../../../nandlib/include" --diag_warning=225 --abi=eabi --preproc_with_compile --preproc_dependency="aic31.pp" "C:/Program Files (x86)/Texas Instruments/C6748_StarterWare_1_20_01_01/examples/evmC6748/mcasp/aic31.c"
The current directory is invalid.
gmake: *** [aic31.obj] Error 1
I searched all over my C: drive but I can't find a subdirectory named ipclite.How/where do I obtain the missing files that were installed as part of CCS v5.1 installation?