We have made an incremental release (v 02.00.00.05) for AM335x on Dec 23rd 2011. The following are the major updates in this release,
For more information please refer the release notes.
Hi Baskaran,
The release notes mentions that the updated linker command files for usb CCS projects can be obtained from here:
https://gitorious.tif.ti.com/starterware/starterware-src/trees/master/build/armv7a/cgttms470_ccs/am335x/beaglebone/usb_dev_msc
But these do not seem to be accessible. Can you please verify?
Regards,
Madhvapathi Sriram
Thanks and regards,
Thanks for the comment Sriram.
Since this is internal link it may not be accessible outside TI. I have uploaded the files in Processor wiki and updated the release notes with this link to download these files.
Regards
Baskaran
My AM335X EVM board can't work normally Based on StarterWare,but it can work based on linux or android system。And,I find that MLO which i get from StarterWare example can not boot the board。I spent a day to try,Phenomenon are all the same。On the other hand,StarterWare work Normally on my BeagleBone board。 why?
Hello Zhu,
I don't have EVM board, but if I understand right the SW3 switch has to be set properly to select the right boot mode. Just a thought that might help.
Valentin