Hi,
I am using LogicPD's Zoom eXp Am1808 board with latest Starterware firmware. I am using CCSv5.1 with CodeSourcery GCC to compile evmAM1808 examples for USB Host.
To be specific, I am working usb_host_mouse example. I referred http://processors.wiki.ti.com/index.php/StarterWare_USB#HID_Host_Class.
On running, the board is not able to detect the mouse connected on J6 USB-mini OTG port. On the LCD screen left most bottom corner I see "No Device". Even the optical mouse's LED is not glowing.
Do we need to connect external power supply to power up the mouse ??
Same thing happens with usb_host_msc example when I connect a flash drive to the same port. I get FR_NOT_READY on PC terminal screen.
So in order to run any host application on this board, do I need to power up my device externally ?
Regards,
Rohit