In AM1808 StarterWare 1.00.03.03
There are currently three copies of ustdlib.c and ustdlib.h in evmAM1808/examples, with the following differences:
- usb_dev_bulk
- oldest: commented as "Stellaris" - grlib_demo
- newer: commented as "Sitaraware" - usb_dev_serial
- newest: "Sitaraware" + several changes to "unsigned long" from "unsigned int"
Also, Ustdlib_api is included in the Modules section of the chm documentation file...
Shouldn't this all be a single copy of library code?