Hello,
I have several questions about the starterware Uartecho example for Beaglebone board.
1) The example uses the UART0, however, UART0 is not connected externally where a jumper can be placed. Do we need to do extra work to connect UART0 tx to the UART0 rx?
2) I am debugging the example by stepping into it and I notice that the FCR value at mode A and the operational node are not successfully written. it fails to write the FCR register value in the UARTFIFOConfig function in the uart_irda_cir.c (driver file) when I set a break point on the UartFIFOConfigure() function in the uartecho.c file. The fcrvalue is 0x57, however, in the memory address it displays 0xC1 after being written.
3) In the interrupt service routine part, the rx only receives the last character "." in the end, because it only triggers interrupt once at the end. In the ISR, the FCR/IIR value is always C2, does this mean the RX FIFO is always being reset?
Thanks a lot!!!