See below when I do "Build Project" on the example rtcClock in our AM3352 board. Where to download these files ... what can I do?
**** Clean-only build of configuration Debug for project rtcClock ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k -j 4 -s clean
Could Not Find C:\ti\AM335X_StarterWare_02_00_01_01\binary\armv7a\cgt_ccs\am335x\evmAM335x\rtc\Debug\rtcClock.out
'Finished clean'
' '
**** Build Finished ****
**** Build of configuration Debug for project rtcClock ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k -j 4 -s all
'Building file: C:/ti/AM335X_StarterWare_02_00_01_01/examples/evmAM335x/rtc/rtcClock.c'
'Invoking: ARM Compiler'
'Finished building: C:/ti/AM335X_StarterWare_02_00_01_01/examples/evmAM335x/rtc/rtcClock.c'
' '
'Building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmAM335x/rtc/Debug/rtcClock.out'
'Invoking: ARM Linker'
<Linking>
error: cannot find file
"../../../../../../../binary/armv7a/cgt_ccs/am335x/drivers/Debug/drivers.lib
"
error: cannot find file
"../../../../../../../binary/armv7a/cgt_ccs/am335x/system_config/Debug/syste
m.lib"
error: cannot find file
"../../../../../../../binary/armv7a/cgt_ccs/utils/Debug/utils.lib"
error: no input section is linked in
undefined first referenced
symbol in file
--------- ----------------
Entry
error: unresolved symbols remain
warning: entry-point symbol "Entry" undefined
warning: no suitable entry-point found; setting to 0
error: errors encountered during linking;
>> Compilation failure
"../../../../../../../binary/armv7a/cgt_ccs/am335x/evmAM335x/rtc/Debug/rtcCl
ock.out" not built
gmake: *** [../../../../../../../binary/armv7a/cgt_ccs/am335x/evmAM335x/rtc/Debug/rtcClock.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****