Hello,
I am struggling with getting the RTOS to run on the BeagleBone Black. I can get no further than the "Jumping to StarterWare Application" part. Here it apparently hangs.
Does the SYS/BIOS require a different MLO, bootloader than the standard StarterWare examples?
My setup:
I am not using an emulator or a JTAG
Using 6-pin header to USB cable for serial output, via TeraTerm.
BeagleBone Black Rev B
CCS Version: 5.5.0.00077
AM335X_StarterWare_02_00_01_01
Latest patch for BBB has been installed
Built bootloader app and renamed the boot.bin to MLO
I can build and run the StarterWare example projects
Here's what I have done:
Created new Workspace
TI Resource Explorer>ARM>AM3359>GNU Target Examples>Generic Examples>Hello Example
Import the project.
Build the project. Creates a "hello_AM3359_CortexA.out"
Used tiobj2bin to convert .out file to .bin file
Renamed "hello_AM3359_CortexA.bin" to "app"
Used MLO that worked with all StarterWare example code
I have compiled different example projects under SYS/BIOS but they all fail at the same place, and appear to hang at the Jumping to StarterWare Application. I am not positive that it is hanging, but I do know that I can see nothing happening on the TeraTerm, where my serial output is.
Any ideas?