Hi,
I'm trying to understand the 0x6A75 value in the DSCOUNT field of DEEPSLEEP_CTRL. Our board uses a 19.2 MHz oscillator as opposed to the more common 24 MHz one.
Based on my experminentation, 0x6A75 == 27253 corresponds to a delay of 5.68 ms, indicating that it's actually counting at a frequency of MOSC/4 == 4.8 MHz. For a 24 MHz oscillator, the same number of cycles would amount to a 4.54 ms delay, which seems excessive; I would expect a value in the ballpark 1 - 1.5 ms.
Where does the 0x6A75 value come from, and is the "excessiveness" there to cover temperature changes, process variations, different manufacturers etc?
Thanks,
Orjan