(ICE-Board AM3359, indsdk 1.1.0.1)
Hello,
the UART RX works with no problem, because i can use CharGetNonBlocking().
On the TX line, there´s at the moment the CharPut function, which works (data send correctly) but the ISR stocks in the while() insctruction of this function. When i simply tried to use CharPutNonBlocking, then the data is corrupted, because, i assume, the new data overwrite the current TX buffer, which is at this moment not completly transmitted.
Can anyone give me a hint what should i do? Something like a longer FIFO buffer? Has someone an example of a UART config, which would be helpful.
thanks