My questions are centered around what RTOS kernel & middleware to choose given our connectivity requirements.
1. Must support Ethernet (TCP, UDP,FTP, DHCP, Static IP, ARP, HTTP, Ping, Telnet protocols to name a few).
2. Must support Ethernet over USB.
We have AM335x GP EVM,This is the scenario.
USB0:Configured as Device,must connected to the HOST PC.
USB1:Configured as a host,will capable to connect the devices like Wifi & 3G modules.
1.Is that the lwIP TCP/IP stack and Starterware USB library would be able to satisfy the above two requirements?
2.Is the Starterware USB Library used with SYS/BIOS?
3.IS the Starterware USB LIbrary supports etherent over USB?
4.Is lwIP TCP/IP stack supported by SYS/BIOS RTOS? Has this stack been ported to SYS/BIOS or should we do that on our own?
5. If SYS/BIOS is not the right choice for our requirements, can you recommend an alternative solution?
6.Are there any example projects that show how Starterware library APIs can be called from SYS/BIOS kernel ?
The Host PC should accessing the web over USB0,Please guide me any approach should follow.
Thanks & Regards
Rama Krishna