Hi , I need to use UART2 and UART4 on beaglebone black with starterware. Is beaglebone plafform starterware code support uart2 and 4
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi , I need to use UART2 and UART4 on beaglebone black with starterware. Is beaglebone plafform starterware code support uart2 and 4
Moving to StarterWare forum.
Best regards,
Miroslav
Hi Terry,
Currently the beaglebone platform code does not have support for UART2 and UART4 instances. You can refer the UART0 Pinmux and Clock functions defined under platform\beaglebone\uart.c or platform\evmskAM335x\uart.c as reference to define the Pinmux and Clock functions which you need to get the peripheral to transmit/receive data.
Additionaly you can refer the following thread related to pinmuxing
http://e2e.ti.com/support/embedded/starterware/f/790/t/282104.aspx
Regards
Anant Pai
Thanks for you help.
http://e2e.ti.com/support/embedded/starterware/f/790/p/356981/1254943.aspx#1254943
regards
terry