Hello,
I’m trying to run the mcspi example of the starterware of the “am335x_sysbios_ind_sdk_1.1.0.6” on the "AM3359 Industrial Development Board". I’ve successfully built the example project in CCSV6.
When I try to run it on the board no UART outputs are printed in the hyperterminal. I’m receiving only the booting messages of the board.
I suggest the UART-functions in the example project uses the wrong UART. (ConsoleUtilsPrintf() etc)
My question is,
how to get the mcspi example project working on the AM3359 IDK?