I'd like to ask a question:
I have a Starter Kit and a homemade development board of AM335x.It in the hardware part is the same.It runing in the RGMII 1000BT mode.
homemade development board:
When running in the WINCE or Linux,the AM335x can received from PHY(AR8031).But it is failed when I runing in the Starterware(enteLwip).No data has been received.In the CPSW_STATS(0x4A100_900) ,it is always zero.But it's possible to transmit.I can received from am335x on the computer.
Starter Kit:
When running in the Starterware(enteLwip),the value of CPSW_STATS(0x4A100_900) has been growing.And I can transmit and receive on the computer.
Test:
1.I read the register from AR8031.He two are the same.
2.I read the register of PinMux from am335x.He two are the same.
So I don't know what to do.
Starterware is 02_00_01_01.Does it have a bug? Can you help me?