Hi All,
We are using AM335x for one of our system development where system boot time is very stringent. We are expecting the unit to boot in 500ms time. We are exploring multiple options to achieve this. Need inputs to decide on this. We want to use TI starterware bootloader to achieve this.
Following are the available options and would like to know which one would give the best boot performance.
1. TI starterware boot loader booting from NAND flash
2. TI starterware boot loader booting from SD card
3. TI starterware bootloader booting from SPI NOR flash
Let me also know if there is any data for boot up time using u-boot?
Regards,
Seetaram