Issue: sample programs not able to start vie IDE
Hardware: TMDXIDK437X Rev: A
CCS: 6.1
SDK: AM437x_sysbios_ind_sdk ... 02_00_00_02
SYSBIOS 6.40.3.39 Real Time Operating System
xdctools_3_30_04_52_core_win32_nojre
Compiler GNU v4.7.4 (Linaro)
Build: ok
Gel: runs ok
program (led_toggle) load: ok (main label visible in ASM)
cpu runs after download, no JTAG control, no breakpoints possible
Target configuration Connection Test: ok, no errors
wondering: project settings show Generic CortexA8 Device (should it not be CortexA9?)
tried other variant (Generic Cortex A9 Device and IDK_AM437x [Cortex A]), but build failed
Viewing various Memory locations also failed.
I have three suspicious aspects then
a) the JTAG connection/settings
b) the project build settings (which are the original ones from the IDK SDK)
c) platform does not match SDK
appreciate some comments in case anyone also works on the AM437x IDK
thanks
Thorsten