Hi,
I can run/boot several examples from the SD card successfully. Now I'm trying to boot from the serial connection, using bootloader in debugger anf a serial connection via a FTDI 3v3 cable. The bootloader starts well but when I start a (bin)file to download it fails. My only question at this point is: Is the bootloader from AM335X_Starterware_02_00_01_01 suitable for serial booting the BeagleBoard Black? Or will I need to adapt the code? I already have the patch installed!
k.rgds.,
Laurent