I've problems to use your mmcsd examples inside of our sysbios project for integrating of a filesystem. There is one example SD_SPI_Flasher, which is written as Sysbios project (not only Bootloaderproject). But it isn't using the cache:
Cache.enableCache = false; // inside of cfg file
If I switch on the cache, it doesn't work anymore! The read first block of sd-card is getting wrong data (cache problems?) with no file-system as result.
1. How this example must be changed to work with using cache?
2. Can I use the edma instead of polling the mmcsd-registers by cpu?