I have downloaded AM335X starterware and installed on to my Windows 7 64 bit. Upon browsing the installed directory I found that it has some projects under “C:\ti\build\armv7a\cgt_ccs\am335x\evmAM335x”.
Upon importing and compiling below project
C:\ti\AM335X_StarterWare_02_00_01_01\build\armv7a\cgt_ccs\am335x\beaglebone\gpio
I had problems with
- Include search path under Build->ARM Compiler->Include options and
- File Search path under Build->ARM Linker->File Search Path
I have resolved compiler include and linker file search path by editing the path accordingly.
After linking, I am getting below error:
**** Build of configuration Debug for project gpioLEDBlink ****
"C:\\ti_ccs_6_1_0\\ccsv6\\utils\\bin\\gmake" -k -j 8 -s all
'Building file: C:/ti/AM335X_StarterWare_02_00_01_01/examples/beaglebone/gpio/gpioLEDBlink.c'
'Invoking: ARM Compiler'
'Finished building: C:/ti/AM335X_StarterWare_02_00_01_01/examples/beaglebone/gpio/gpioLEDBlink.c'
' '
'Building target: C:/ti/AM335X_StarterWare_02_00_01_01/binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Release/Srini.out'
'Invoking: ARM Linker'
<Linking>
'Finished building target: C:/ti/AM335X_StarterWare_02_00_01_01/binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Release/Srini.out'
' '
error: failed to read
"../../../../../../../binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Debug/gpi
oLEDBlink.out"
Use of uninitialized value $str in pattern match (m//) at XML_TI_OFD.pm line 2144.
Use of uninitialized value $targ_num in hash element at XML_TI_OFD.pm line 1323.
Unexpected target: unknown at script/mkhex4bin.pl line 261.
fatal error: cannot open input file
"../../../../../../../binary/armv7a/cgt_ccs/am335x/beaglebone/gpio/Debug/gpi
oLEDBlink.out": No such file or directory
The system cannot find the path specified.
' '
**** Build Finished ****
Any input on this?
Regards
Srinivasa