Hi,
I want to create a new project on AM4379 sitara series. we are using ccs v6.
To do this i selected AM4379 and selected a sysbios typical example project template.
To this project, I included the following paths to the project.
After this, I tried to acces functions of the include files from the main file.
when i compile the files, it gives the following error.
**** Build of configuration Debug for project JTA_gpio ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
making ../src/sysbios/sysbios.aa9fg ...
gmake[1]: Entering directory `C:/Users/jinu.andrews/workspace_v6_1/JTA_gpio/src/sysbios'
gmake[1]: Nothing to be done for `all'.
gmake[1]: Leaving directory `C:/Users/jinu.andrews/workspace_v6_1/JTA_gpio/src/sysbios'
'Building target: JTA_gpio.out'
'Invoking: GNU Linker'
"C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-4_8-2014q3/bin/arm-none-eabi-gcc.exe" -mfloat-abi=hard -Dam4379 -g -gdwarf-3 -gstrict-dwarf -Wall -Wl,-Map,"JTA_gpio.map" -nostartfiles -static -Wl,--gc-sections -Wl,--defsym,STACKSIZE=0x18000 -Wl,--defsym,HEAPSIZE=0x400 -o"JTA_gpio.out" "./main.o" -Wl,-T"./configPkg/linker.cmd" -Wl,--start-group -l"c" -l"gcc" -l"m" -l"nosys" -Wl,--end-group
./main.o: In function `main':
C:\Users\jinu.andrews\workspace_v6_1\JTA_gpio\Debug/../main.c:131: undefined reference to `MMUConfigAndEnable'
C:\Users\jinu.andrews\workspace_v6_1\JTA_gpio\Debug/../main.c:132: undefined reference to `CACHEEnable'
C:\Users\jinu.andrews\workspace_v6_1\JTA_gpio\Debug/../main.c:139: undefined reference to `GPIOAPPPINOBJ_DEFAULT'
..................
is there anything else need to be added in this project to get compiled ?