Hello,
I am trying to create a macro library for the first time.
I follow step by step the indications written in ARM Assembly Language Tools v5.1 User's Guide.
I got an assR18.lib file after the command:
c:\ti\ccsv6\tools\compiler\ti-cgt-arm_5.2.2\bin\armar.exe -@assRlibCommands.cmd
Then I placed the assR18.lib file in the Include directory and I cleaned the project.
I got the following warning:
#10189-D archive symbol directory is missing from archive "../include_appli/assR18.lib"
If I replace in source file “.Include assR18.asm” by “.Include assR18.lib” There is no illegal mnemonic error and the compilation seems to be good except that the project is not remade because of error:
gmake: Target `all' not remade because of errors.
**** Build Finished ****
The compiler does not tell us anything about the error.
I tried to build an archive with the following command:
c:\ti\ccsv6\tools\compiler\arm_5.1.5\bin\armlibinfo.exe -o=assR18_Arch.lib assR18.lib
I got a file with only one line inside:
!<arch>__TI_$$LIBINFO/ 1441178127 0 0 0 0
What can I do?
Thanks a lot for your help
Jerome