Hi,
I want to test ethernet test application provided with AM437x SDK. For this, I loaded tcp echo application in CCS.
On hyperterminal,I can see that application performs phy configuration and IP acquisition and also an ip address is announced.
Now i want to run the enet client code from Windows PC.
The path for enet client code is mentioned below.
C:\ti\am437x_sysbios_ind_sdk_2.0.0.1\sdk\starterware\tools\enet_client
On the SDK user manual, it is mentioend to follow instructions under host_apps/enet_client. in that path on the readme text the following instructions were mentioned.
1. Copy client.c and data.txt to the linux host machine.
2. Compile the client program $gcc client.c -o client
3. Run the executable $./client <ip-address-announced-by-the-server>
In the above mentioned steps, what is data.txt file?
Also how can we run this application from a windows PC?