This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Filippo,
Before continuing, please take a look at the latest Processor SDK release for AM335x which was just released. This release has a starterware package which has updates (pdk_am335x_1_0_0\packages\ti). You would need the latest CCS 6.1.1 to work with this release.
To demonstrate based on the lcdc raster example in this release I was able to access LCD_CONTROLLER_RASTER_TIMING_0 at location 0x4830E02C and manipulate the values in the CCS memory browser.
Which specific memory location are you trying to access? 0x4830E000?
Lali
Domenico,
Attached is my screenshot. This is the example from ProcessorSDK run on the AM335x GP EVM.
C:\ti\pdk_am335x_1_0_0\packages\ti\starterware\examples\lcdc\raster
Are you running this on a custom board?
I notice that you are running the example of the older starterware package. Could you please try this from the ProcessorSDK package? The link is in my earlier post.
Lali
I'm using the standard file GEL.
I can load the software and run the software with Sys / Bios, I manage myself, the serial, but the task can not log all'LCDC.
I have three versions of the latest CCS is 6.1.1.00022.
the behavior is similar.
My reference is the document SPRUH73L of February 2015.
For example, the register CM_PER_L4FW_CLKSTCTRL displayed on CCS is not described on the documentation and so also others.
There is a correct document? Complete?
Filippo,
CM_PER_L4FW_CLKSTCTRL is not exposed in the TRM. Please see these threads.
https://e2e.ti.com/support/embedded/starterware/f/790/p/397867/1411218
https://e2e.ti.com/support/arm/sitara_arm/f/791/t/200835
Lali
ok,
I solved it with the LCD. For me, the documentation is not very precise.
Greetings
Filippo