When can we expect to have a working Starterware example for the Vivante Corp. GC320 accelerator sub-system that is included on the SOC AM5728 (for the X15)?
The available documentation appears to be incomplete ~ like the following are missing from the AM572x (spruhz6d) technical reference manual:
- setting-up the Host interface.
- documentation for using the Graphics pipeline (commands needed).
- drawing and scaling functionality information.
- pixel engine commands.
Starterware code would be the ideal jump-point for me to begin using this sub-system.
Thanks in advance!
Dean Wedel