What parameter settings do I need to initialize the SPI device connection to J3 in the following function:
McSPIInit(spiId, spiClockDiv, spiDir, chMode, chNum);
I'd like to uses the largest clock divisor possible (hence the slowest speed possible) as I'm using an EVAL CARD to EVAL CARD lab setup.
Sounds like spiClockDIv should be set to 255. How about spiId, spiDir, chmode, and chnum?