Greetings E2E Community,
I am currently working on a project involving the AM3359. Currently, it is still in the evaluation stages. The hardware that I'm using is the ICE v2 dev board with the AM3359. I already have the SYS/BIOS Industrial SDK, and its prerequisites, installed and setup. Also, I have a basic CCv6 project based on a typical SYS/BIOS template with Starterware source and header files for I2C. I've attached a zip file with my CCv6 project. Before I go any farther, could someone give me some advice as to how to configure the AM3359 as an I2C slave using Starterware? Basically, I want to create a SYS/BIOS application for the AM3359 that can be an I2C slave, and I'm looking for advice as to the proper way forward before jumping down the rabbit hole :)
Sincerely,
Daniel1055.Test.zip