Hi all:
I am working with AM3354 using CAN and LCD, but I got an abort exception when I using LCD with raster mode DMA!
Here is the way I'm using LCD.
I'm using Raster mode DMA , two DMA buffer , buffer1 for FRAME0 and buffer1 for FRAME1 . UIBuffer for app.
When I stop Flush the UIBuffer to the buffer0 buffer1 or don't change the content of the UIBuffer(still Flush UIBuffer to buffer0 and buffer1) , then I got no abort exception.
But ones I start Flush UIBuffer to the buffer0 buffer1, I got the abort exception later (about 10 to 20 min).
Is it maters changing the buffer1 value when the DMA using the buffer1?