hi all,
StarterWare 02.00.01 for AM335X,download from software-dl.ti.com/.../index_FDS.html.
Code Composer Studio Version: 6.1.3.00033,download from processors.wiki.ti.com/.../Download_CCS.
Then bulid the starterware project (eg,D:\ti\AM335X_StarterWare_02_00_01_01\build\armv7a\cgt_ccs\am335x\drivers), using default settings.
It occur that serious errors made the build terminate as following shows.
Errors occurred during the build.
Errors running builder 'CDT Builder' on project 'drivers'.
java.lang.NullPointerException
How to handle that ? Thanks a lot for your help!
When build the starterware project with CCS v6.1.2, there are also other tough problems, such as losing runtime support libray -- rtsv7A8_A_le_eabi.lib.
How to generate the library, what each part symbol means ? In new version CCS, only the library rtsv7A8_T_le_n_v3_eabi under installing directory.
Thanks again !