Hi,
I use idkam437x with sdk 2.1.1.2. I used to have problems with getting a number of words currently present in ADC0 fifo0 buffer. When I used TSCADCGetFifoWordCount() function with a parameter TSCADC_FIFO_SEL_0 a return value was zero. When passing TSCADC_FIFO_SEL_1 parameter, the number returned was correct. In source code of the function, the fifoSel parameter is decreased by one, what might be an error in the TSCADCGetFifoWordCount source code. Am I right?
Thanks
JJ