Hi,
We are working on industrial based project based on AM4379BZDNA100 chip.We used sysbios_ind_sdk_2.1.0.1.By following design similar to AM437x IDK board we manufactured Revision 1 custom boards on September 2015 using the available bootloader with sysbios_ind_sdk_2.1.0.1 the boards were booting perfectly in QSPI boot mode. But same boot loader code not working on Rev B boards manufactured on MAY 2016. The boards are booting from QSPI flash but it is getting stuck whenever code tries to write to QSPI register which lies in memory map region 0x3000000 .We haven't changed anything related to QSPI booting on our board. Also cross checked the functionalities of QSPI,DDR etc saparetly using test codes and all are working fine.
What could be the reason behind this? Is there anything changed on Boot Rom code on this chips we received on may 2016 and September 2015?
Regards,
Jinu Jacob Andrews