Hello,
i'm using CCS Version: 6.1.2.00015 , starterware 02_00_01_01.
i'm trying run code on the BBB as fast as possible in order to have a minimum latency between inputs and outputs.
and i'm not able to go under 1uS in my project.
i tested a simple delay function
static void Delay(volatile unsigned int count)
{
while(count--);
}
and using the same MLO, the delay function is 40x faster in the demo project example than in the gpioLEDBlink project example.
as far as i read in the code of the bootloader the configuration of the OPP and PLL are already done in (MLO) to the max
so my question is what i have to configure in my app to get the same performances as the demo project?