Hello All,
I am currently working with the TI ICE version 2 board and I am trying to rebuild the bootloader (From the AM335x SYSBIOS Industrial SDK 01.01.01). I am having some trouble rebuilding the given project within the SDK. Some of the instructions in the AM335x SYSBIOS Industrial SDK 01.01.01 User guide are hard to follow for me would appreciate someone helping me out with the following:
1. How do I Set build configuration for dependant projects as "FixedPoint"?
2. Import dependent starterware projects. They are drivers, platform and mmcsdlib?
3. Build dependent projects in CCS?
4. Set predefined macros?
5. Set the post build script arguments properly?
When I try to build the project I get the following error.
Errors occurred during the build.
Errors running builder 'CDT Builder' on project 'boot'.
java.lang.NullPointerException
When I first open the project there is no RTSC configuration.