example profinet_slave_RT can running alone;example enetLwip_sysbios can running alone too.
then I would procedure of enetLwip_sysbios to procedure of enetLwip_sysbios profinet_slave_RT.
With the emulator online simulation program is good,
The program to burn into the spi flash on electricity can run for the first time, but the second can't run on electricity.
I did an experiment:
this is in int main(void);If this program is very good, burn to the spi flash can run inside.
but
the Lwip_SetDelay() in enetlwip.c;
to burn into the spi flash will appear on the first electric program can run, but the second can't run on electricity.
These two programs.. Spi. Bin file is not as big.
Why is this case?
Could you give me your expert advise?
Thank you for your answer first.