My setup:
AM3359 ICE V2
CCS V 6.1.3
SYSBIOS IND SDK 2.1.1.2
Hi,
i am using the ICE v2 with the Profinet_RT example from sysbios ind sdk 2.1.1.2. I modified this example for SPI master communication using SPI1. Now i need two slaves on the SPI1. Because of only having one chip select pin on connector J3 i want to change the pinmux. I used the pinmux tool v4 and opened the pinmux configuration in C:\ti\sysbios_ind_sdk_2.1.1.2\sdk\starterware\tools\pinmux_config\am335x\icev2_config which seems for me to be the standard configuration used in the sdk examples. I read about it here:
I changed SPI1 pinmux to a new valid configuration and downloaded the starterware files created by the pinmux tool (am335x_gpevm_pinmux_data.c and am335x_pinmux.h) I renamed the first one to "am335x_icev2_pinmux_data.c according to the following post and changed the "gpevm" at the end of the file to "...gIceV2...", also according to the following instruction file:
Then i replaced the original two files in C:\ti\sysbios_ind_sdk_2.1.1.2\sdk\starterware\board\am335x.
Now the next step would be to rebuild/recompile those starterware library/source files i guess? But how to do this ? In the instructions for pinmux modifications in the .pdf above it is described for the pdk and not for the starterware within the sysbios ind sdk. Would you please help me how to do this ?
Thanks in advance
Michael