Hi,
I use IDKAM437X with CCS 6.1.2 and sysbios 2.1.1.2. In SDK packet within starterware section there is a bootloader project. I set all build-configurations in other projects according to bootloader's 'Dependencies' section. In the end of build process, the following errors occur:
I tried some of the solutions mentioned on this forum but none of them worked for me. Could you please suggest me what the problem is?
There are two things that concern me about OCMCRAM memory:
- should the start address in post-build steps be equal to 0x40300000 instead of 0x402F0400?
- should the length of OCMCRAM section in linker file (AM437x.lds) be equal to 0x00040000 (256kB) instead of 0x00010000(64kB)?
Thank you in advance!
JJ