Dear Friends,
I am running a modified version of the usb_dev_bulk example on the C6748_LCDK.
The maximum throughput I am getting is about 2.3Mbytes per second (18Mbits per second), while USB 2.0 allows up to 480 Mbits per second.
I am using packet size of 1024 bytes (maximum allowed).
Has anyone got better throughput?
Is this a Startware driver issue?
Is there a document describing the C6748 USB registers?
I saw the similar post from 2014 but there was no answer.
Thanks,
Avi Tal.