Tool/software: Starterware
Hi All,
- The Application present in "AM335X_StarterWare_02_00_01_01/examples/evmAM335x/uart/uartEcho.c" file, has two features Mentioned in Comments.
Running the Example:
On executing the example:
1) A string is displayed on the serial console of the host machine.
2) The user is then expected to key in data on the serial console.
The keyed in data are immediately echoed back by the application
and are visible on the serial console.
- first feature is i am understanding.
Question: The 2nd feature of the application code is i am not finding entire code (Sorry for stupid question)?.
- Please specify the Code for the 2nd feature of uartEcho.c file, where the echoed back code present?
Regards,
Vamsi.