Tool/software: Starterware
Hey everyone,
i am facing some difficulties trying to control the gpio pins...
// #define GPIOP8_04 (GPIO_1_7) //pin:P8_04,mode7:gpio1[7] #define PINGP1 (7) #define GPIOP8_07 (GPIO_2_7) //pin:P8_07,mode7:gpio2[7] #define PINGP1_2 (7) #define GPIOP8_22 (GPIO_2_22) //pin:P8_26,mode7:gpio2[22] #define PINGP2 (22) // the following code is to toggle the pins defined above // L3L4_driver_init(); L3L4_clock_domain_open(); GPIO1ModuleClkConfig(); GPIO2ModuleClkConfig(); GpioModuleEnable(SOC_GPIO_1_REGS); GpioModuleEnable(SOC_GPIO_2_REGS); //pin mux setup // P804 GpioPinMuxSetup(GPIOP8_04, 7); GPIODirModeSet(SOC_GPIO_1_REGS,PINGP1,GPIO_DIR_OUTPUT); // P807 GpioPinMuxSetup(GPIOP8_07, 7); GPIODirModeSet(SOC_GPIO_2_REGS,PINGP1_2,GPIO_DIR_OUTPUT); // P822 GpioPinMuxSetup(GPIOP8_22, 7); GPIODirModeSet(SOC_GPIO_2_REGS,PINGP2,GPIO_DIR_OUTPUT); // while(1) { GPIOPinWrite(SOC_GPIO_1_REGS, GPIOP8_04, GPIO_PIN_HIGH); Delay(0xAFFFF); GPIOPinWrite(SOC_GPIO_1_REGS, GPIOP8_04, GPIO_PIN_LOW); Delay(0xAFFFF); // GPIOPinWrite(SOC_GPIO_2_REGS, PINGP1_2, GPIO_PIN_HIGH); Delay(0xAFFFF); GPIOPinWrite(SOC_GPIO_2_REGS, PINGP1_2, GPIO_PIN_LOW); Delay(0xAFFFF); // GPIOPinWrite(SOC_GPIO_2_REGS, GPIOP8_22, GPIO_PIN_HIGH); Delay(0xAFFFF); GPIOPinWrite(SOC_GPIO_2_REGS, GPIOP8_22, GPIO_PIN_LOW); Delay(0xAFFFF); // }
The problem with this code is that the leds i connect to my beaglebone white do NOT turn on and off...instead there seems to be only a very dim light in only one of the leds (the second one, P8_07), which is also constantly on...Now the resistor i use is 470 Ohm and i am pretty sure that is not too much, as if i connect the led with pin 4 in P9 header (3.3V output) instead of the gpio pin, the led turns on just fine..
Could someone help me out? Is the pin mux not done properly? What else shoud i try?
Thanks in advance