• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » All Tags » OMAP3530
Share
Embedded Software
  • Announcements
  • Android Android
  • BIOS BIOS
  • Linux Linux
  • Multimedia Software Codecs Multimedia Software Codecs
  • StarterWare StarterWare
  • WinCE WinCE

Browse by Tags

Embedded Software

Welcome to the Embedded Software Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
OMAP3530
  • 6446
  • 6467
  • AM/DM37x
  • am1808
  • am18x
  • am3517
  • android
  • android rowboat
  • arago
  • ARM
  • ARM-A8 WINCE BSP
  • audio
  • beagleboard
  • boot
  • bootargs
  • BSP
  • c64x+
  • cmem
  • code Composer studio
  • codec
  • codec engine
  • codecs
  • Da Vinci
  • DaVinci
  • daVinci dm365
Related Posts
  • Forum Post: Mistral OMAP3530 EVM - don't understand when to use .raw files delivered w/ BSP or to use files created with build??

    Marc DAmato Marc DAmato
    All, Do you have to use new EBOOTXXXX.bin each time you rebuild an OS runtime image or can you stick w/ the ones delivered w/ the BSP package. I'll use BSP 6.13.0 OMAP3503 as an example BSP - bspdemo_omapwince_06_13_00, comes w/ EBOOTXXXX.bin, NK.bin, XLDRXXXX.bin, and TIEVM3530-XXXX.raw, where...
    on Mar 17, 2010
  • Forum Post: When will the BSP6.14 be released?

    Sung-IL Sung-IL
    Hi all, Could you please let me know when will the WinCE BSP6.14 version for OMAP3530 be released? And when will the WinCE BSP for AM3517 be released? Thanks and Best Regards, SI.
    on Apr 20, 2010
  • Forum Post: WinCE/OMAP3530 OpenGL app hangs after system enters systemidle (powerstate-D2)

    muragesh math13999 muragesh math13999
    hi, I am executng an OpenGL application on OMAP platform, The application works properly till the device enter systemidle mode, But after systemidle mode the OpenGL app hangs. the other wince applications are working properly even after the systemidle mode. Why the OpenGL app should hang...
    on May 6, 2010
  • Forum Post: Re: WinCE/OMAP3530 OpenGL app hangs after system enters systemidle (powerstate-D2)

    Mauricio Sanchez15270 Mauricio Sanchez15270
    Hi Muragesh, Which version of the BSP are you using (You can use the icon in the control panel for this)? When you say that the application is hanging, does it mean that after taking it out of idle (mouse/keyboard event) it does not start again? Do you need to reboot you platform? What is the behavior...
    on May 6, 2010
  • Forum Post: How to adapt BSP to an OMAP-3530 based board ( a board derived from Beagle Board )?

    arthur14426 arthur14426
    Hello everyone, An OMAP-3530 based board is used in our project. The board (ICETEK-OMAP3530-MINI V3) is get from RealtimeDSP( www.realtimedsp.com.cn ) , which derived from Beagle-Board , and It has more memory( 256M Byte mDDR and 512M Byte Nand Flash ) , and has a VGA-Adapter subboard ( an VGA DAC...
    on May 13, 2010
  • Forum Post: Re: how to suspend the ehci driver

    Rich Chen Rich Chen
    USB EHCI suspend/resume looks like still a open issue on WinCE BSP 614. Is there any plan on fixing this open issue? This affects the power management scheme if it is not fixed. Best Regard, Rich
    on May 14, 2010
  • Forum Post: camera sensor mt9v022 with omap3530

    Yong Wang47643 Yong Wang47643
    hi, how can i make omap3530 work with the camera sensor mt9v022 through the ISP? is there a right driver for the sensor?
    on Jun 9, 2010
  • Forum Post: Re: codec engine problem!

    Wen Liu44416 Wen Liu44416
    Hello , I have met the same problem. in xdcpaths.mak : CE_INSTALL_DIR := /home/newton/dvsdk_3_00_02_44/codec_engine_2_24 this is my log failure newton@ubuntu:~/dvsdk_3_00_02_44/codec_engine_2_24/examples/ti/sdo/ce/examples/codecs$ make make -C viddec1_copy all make[1]: 正在进入目录 `/home/newton...
    on Jun 14, 2010
  • Forum Post: Self-Refresh w/256MB of RAM in PM lowest power modes

    Chris R Chris R
    Has the self refresh mode for the LPDDR been tested with the full 256MB that's in the newer beagleboards and EVMs? I know that both newer beagleboards and the OMAP-35x EVMs (e.g. Rev.G) have 256 MB of LPDDR on them. Their POP packages use two LPDDR chips that are each 128MB to create the 256MB...
    on Jun 14, 2010
  • Forum Post: Re: Linux Interrupt jitter, latency

    P.Mutasingwa P.Mutasingwa
    De-bouncing for the GPIO lines was turned off. I turned off various peripherals in the system and was able to narrow down the cause to the gp-timer interrupt. If I mask this interrupt, the jitter disappears. This is the GPTIMER12 on the OMAP. When this interrupt runs it shows up as IRQ-95 in...
    on Jul 9, 2010
  • Forum Post: Re: Unhandled fault: external abort on non-linefetch (0x1018) at 0x4002100c Bus error

    Sue Krebsbach Sue Krebsbach
    You need to make sure that the appropriate McSPI functional ( CM_FCLKEN1_CORE) and interface ( CM_ICLKEN1_CORE) clocks are enabled before reading the McSPI registers.
    on Jul 9, 2010
  • Forum Post: H.264 Baseline Encode DSP Load is high on the OMAP3530

    Dennis E Dennis E
    We're attempting to use the H.264 v.2.01.013 baseline encoder for the C64+ in our OMAP3530 project. We use gstreamer to manage the video capture and encode. Using the dmaiperf plugin for gstreamer, we're seeing over 80% DSP load while encoding D1 (720x480 30fps) 1Mbps video. We believe this is...
    on Jul 23, 2010
  • Forum Post: Re: Problems with eDMA in OMAP 3530

    Michael T Michael T
    Felipe: The SDMA is recommended for peripheral to memory transfers. The OMAP 3530 Tech Ref Manual has an example of SDMA configuration to transfer data between McBSP and External DRAM (Section 9.6.1.2). Any specific reason why you would need to use EDMA instead? Michael T
    on Jul 26, 2010
  • Forum Post: Re: Problems with eDMA in OMAP 3530

    Michael T Michael T
    Philipe: In your McBSP1, which is the transmitter, the receiver is enabled and the enabling of the transmitter is commented out: configure_mcbsp1 () // Enable Receive *(BASE + McBSP_SPCR1) |= 0x00000001; // Enables Transmitter //*(BASE + McBSP_SPCR2) = *(BASE + McBSP_SPCR2) | 0x00000001;...
    on Jul 28, 2010
  • Forum Post: Re: using memory from POOL_alloc

    Chris Norris Chris Norris
    Hi Deepali, Thank you for answering my questions and also for your advice on protecting the buffer. I'm presently using NOTIFY from DSP to GPP to inform the GPP that the DSP has updated the buffer. I use a second NOTIFY from GPP to DSP for GPP to acknowledge that it has read the buffer. This synchronization...
    on Aug 2, 2010
  • Forum Post: Re: Setting up usb in linux kernel for omap3525 and TUSB2551A transceiver

    Michael T Michael T
    Ryan: Attached are new UBOOT header files including your new configuration which I have generated using our Pin Mux Utility software which is available at: http://focus.ti.com/docs/toolsw/folders/print/pinmuxtool.html This was done assuming that you will not need to use the CAM or ETK...
    on Aug 3, 2010
  • Forum Post: Re: Setting up usb in linux kernel for omap3525 and TUSB2551A transceiver

    Michael T Michael T
    Ryan: One additional note. The Pin Mux utility also configures active and standby pad configuration (pull-up / pull-down) and gives you a default based on the type of signal selected. These settings can also be changed using the software. PS: Please mark this post as answered via the Verify...
    on Aug 3, 2010
  • Forum Post: OMAP3530 DSI MIPI video mode

    GregoireGentil GregoireGentil
    Hello, We are trying to make work a 3.5'' display with the following characteristics: MIPI, video mode 2-lane + clock 320(H) x 480(V) (RGB Stripe) 24-bits (R8, G8, B8) VP 500 Line VS 8 Line VFP 6 Line VBP 6 Line VDISP 480 Line HP 380 clk HS 16 clk HFP 12 clk HBP 12 clk HDISP 320 clk...
    on Aug 8, 2010
  • Forum Post: Re: Audio Architecture on OMAP3530

    fabrice saadoun fabrice saadoun
    Deepali, Can you please answer questions a and b with the details I gave you previously? Thanks, Fabrice
    on Aug 8, 2010
  • Forum Post: sdio/mmc2 support on omap3530 on my custom board

    Huai Hellen Huai Hellen
    Hi, all, I now used sdio/mmc2 through an external transiver without direction control. the tranciver we used is txs0108, which is a bidirectional voltage-level tranciver. but now, the sd/mmc2 could not work, I can't detect the sd disk. My question is: is there any problem using txs0108, or I must...
    on Aug 9, 2010
  • Forum Post: Re: Problem of Windows Embedded Compact 7 on TMDSEVM3530

    Sho Masuda Sho Masuda
    Hi, Madhvi. Thank you for your reply. I've already seen the similar question that you attached to your comment, but I didn' t understand that I should burn a bootloader to the flash memory to boot correctly. I edited the Catalog file to add the NAND driver and delete the OneNAND driver...
    on Aug 30, 2010
  • Forum Post: Re: Problem of Windows Embedded Compact 7 on TMDSEVM3530

    Sho Masuda Sho Masuda
    Hi, Madhvi I found I can get EVMFlash Tool from WinCE BSP which can be downloaded from TI website. I will download and install the Tool, and update a bootloader. Thank you for your help.
    on Aug 30, 2010
  • Forum Post: Re: Compact 7 Debug Boot Problem on OMAP3530 EVM

    Sho Masuda Sho Masuda
    Hi Jatin, Thank you for your suggestion. I didn't know that moving the memory around will create problems with video playback and display functionality. I will modify the memory allocation keeping the DISPLAY and the CMEM_DSP as-is and just swapping the NK and RAM around, and try to decrease...
    on Sep 8, 2010
  • Forum Post: Re: Compact 7 Debug Boot Problem on OMAP3530 EVM

    Sho Masuda Sho Masuda
    Hi Jatin, Thank you for your detail information. I was able to boot correctly by just swapping NK and RAM in config.bib. I edited nothing in image_cfg.h. Also, I'm sure that multiple complicated steps would be needed if debug image exceeds 128MB. I will try to exclude unneeded components...
    on Sep 9, 2010
  • Forum Post: USB on board hub not working with android on BB-xm

    kiran nayak kiran nayak
    hi all we have our custom board based on omap3530 soc.. the board has been successfully booted with omap-linux-3.1 and USB is working properly.. but the problem is when we try to boot the rowboat gingerbread with rowboat-kernel-2.6.37 the USB is not working acutlly we tried to measure the voltages near...
    on Jul 30, 2012
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use