• TI thinks resolved

RTOS/TI-RTOS: Cannot get available products window to show anything

Part Number: TI-RTOS

Tool/software: TI-RTOS

CCS Version  Version: 7.1.0.00016  just updated.

This used to work, now not at all

Launch CCSV7 with clean option after update.
Create new Workspace
Project -> New CCS Project
Target MSP430FR5994
Name Test01
Goto
TI_RTOS Examples
Driver Examples
Empty Examples
Empty Project

Next Select TI-RTOS for MSP43X 2.20.0.06
Target:ti.targets.msp430.elf.MSP430X
Platform:ti.platforms.msp430:MSP430FR5994
Build Profile: Release
All the defaults
XDCTools default is 3.32.0.06_core but select 3.5.1.12_core as it is newer.
Finish
Build project
Get errors
Description Resource Path Location Type
error #148: declaration is incompatible with "xdc_Ptr ti_sysbios_BIOS_RtsGateProxy_Proxy__delegate__S(void)" (declared at line 244 of "C:/ti/tirtos_msp43x_2_20_00_06/products/bios_6_46_00_23/packages/ti/sysbios/package/BIOS_RtsGateProxy.h") .xdchelp /Test01 line 7482 C/C++ Problem

Select 3.323.0.06_core
Clean and build
No errors this time
Now select empty.cfg to view
No Available Products Window
Select view - Available products window.
Window opens but tells me there is no RTSC configuration b Filke op0en. But have one open empty.cfg
Apparently it doesn't recognize it
Create new RTSC Configuration File from new file menu  file: Same story
Now what?

  • In reply to Frank Chambers:

    Screenshot.rtfCompressed the screenshot

  • In reply to Frank Chambers:

    Frank,
    I am not sure if you still have this problem, but in case you do I would like to ask you for a screenshot that shows Available Products View and the XGconf view at the same time. Right-click on the CFG script and then choose Open With->XGCONF. Can you post a screenshot of the XGconf view, while Available Product View displays the message that there are no open CFG files?

    If my reply answers your question please mark the thread as answered.

  • In reply to Sasha Slijepcevic:

    It is still a problem but getting curiouser and curiouser.  I have attached a compressed file with two screen shots.  The first illustrates the original problem, which still exists.  In the first one I double cliked the cfg file and got the error., also note that there is no [TIRTOS] after the file name.

    The second screenshot is after opening the cfg file with XGCONF.  Now all is well, it even added the [TIRTOS] indicator.  If I close both instances of the cfg file and then reopen with a double click, in the same sessio.  Available products is ok.

    If I exit CCS and reenter and do the same thing it remebers that it is actuallly a config file.  If I pick a different project the same problem with a double click. open it with XGCONF and it is good to go as a cfg file

    It appears thatthe first time you open a TIRTOS project and double click it doesn't recognize the file for what it is, Once it get s opewned directly by XGCONF it remembers.

    Hope this helps.

    Frank

    AvailableProducts.zip

     
     
  • In reply to Frank Chambers:

    Frank,
    screens shots display an expected behavior. A CFG script can be opened in two different ways: in a text editor as a regular text file or in the XDGconf view. When it's opened as a text file, there is no extra processing that detects which products are used in the project and you get that message in the Available Products view.

    CCS comes with a default action when you double-click on a CFG script. For CCS 7.1, the default action is to open a CFG script in a text editor, but you can change the default, which is what you did.

    If my reply answers your question please mark the thread as answered.