I'm in the process of learning how to program Codec Engine and iUniversal, but one thing that I still have not figured out is how XGCONF gets the information about the EVM to generate a template for a .cfg file. I'm using the c6a816x EVM and at present I have two disparate tools sets, one in Linux for the ARM and a second using CCS4.2.3 in Windows for the DSP. At the moment, one doesn't know anything of the other. This is obviously unworkable. For example, in processing an image, I would like to use ACPY3 to transfer rows and columns from main memory to L1 memory. What from EZSDK may be imported to CCS to indicate the board's, and in particular the C674's, memory map, producing a template for the .cfg file?
Lee Holeva