Hello everyone,I have a problem need your guiding,the problem is shown below
Development environment:CCS3.3.82+xds560plus;
The chip is OMPAL138,but I only use the DSP CORE c6748,ARM part is not used;With DSP/BIOS SYSTEM bios_5.41.02.14;compiler is V6.1.11;
Building is well,but in the linking progress,the error is happened shown below
--------------------------------------------------------------------------------------------------------------------------------------------------------------
[Linking...] "C:\Program Files\Texas Instruments\C6000 Code Generation Tools 6.1.11\bin\cl6x" -@"Debug.lkf"
<Linking>
error: symbol "__stack" redefined: first defined in "C:/Program Files/Texas
Instruments/C6000 Code Generation Tools 6.1.11/lib/rts67plus.lib<boot.obj>";
redefined in
"C:/CCStudio_v3.3/bios_5_41_02_14/packages/ti/bios/lib/bios.a674<boot.o674>"
error: symbol "_c_int00" redefined: first defined in "C:/Program Files/Texas
Instruments/C6000 Code Generation Tools 6.1.11/lib/rts67plus.lib<boot.obj>";
redefined in
"C:/CCStudio_v3.3/bios_5_41_02_14/packages/ti/bios/lib/bios.a674<boot.o674>"
undefined first referenced
symbol in file
--------- ----------------
__STACK_SIZE C:/Program Files/Texas Instruments/C6000 Code Generation Tools 6.1.11/lib/rts67plus.lib<boot.obj>
error: unresolved symbols remain
error: errors encountered during linking; "./Debug/138_dm9000RJ45.out" not
built
>> Compilation failure
Build Complete,
1 Errors, 11 Warnings, 0 Remarks.
-------------------------------------------------------------------------------------------------------------------------------------------------------------
In the file dsplinker.cmd stack is defined as:—stack 0x00000800;
In the .tcf file of BIOS system the stack size is defined 0x0400;
Wish your guiding,thanks