I'm in the process of migrating from DSP/BIOS to SYS/BIOS. I'm using CCS 5.2.0.00069, SYS/BIOS 6.33.05.46, and XDC Tools 3.23.03.53. I've converted my *.tcf file to a *.cfg file (attached (1526.VibrationMonitor.cfg) using the migration tool. None of the tasks in my *.cfg file are displaying in the Outline window. In addtion, CCS 5 is displaying related errors such as:
Description Resource Path Location Type
#20 identifier "UsbComms" is undefined main.cpp /VibrationMonitorSYSBIOS line 1474 C/C++ Problem
when UsbComms is clearly defined in the *.cfg file. This is true for all my tasks.
My (two) memory heaps are also not displaying in the Outline window when they had been previously.
Could someone look at my *.cfg file and let me know why my tasks and heaps aren't displaying? Thanks.