. |
Hi,
from the IPC notify header file there a constant which defines Maximum number of events supported by the Notify module
#define Notify_MAXEVENTS (UInt16)32
I could not use event ID = 33 for example, I had a wired behavior.
My DSP is C6678, bios_6_32_05_54, ipc_1_24_00_16
My question is why there is such constraint? I have 8cores in the DSP and I need at least 64 events to map all the cores together.
Thx
--Chek