CCS 5.2, Sys/Bios 6.33
I want to transfer data from M3 to C28 and vice versa triggered by an interrupt on both parts. While the interrupt on C28 fires when I set the IPC flag 1, the interrupt on M3 does not. The image below shows my settings in Sys/Bios. Actually I am not sure whether the interrupt number must be 80 or 96 and the priority 3 or (3*32). So the values I used might be wrong.
The code in C28 is "CtoMIpcRegs.CTOMIPCSET.all |= 1". What else must be done to make it work?
Thanks and regards,
Walter