I am attempting to create a heap in C55xx SRAM using the DSP/BIOS Config tool. However, when I create the heap in SRAM, then change the value in the Memory Section manager for "Set section for malloc()/free() to SRAM, then attempt to save the file, I get the following error;
The only way to exit the Config tool is to cancel without saving the file. After doing this, when I then try to re-open the file, I get the following:
What am I doing wrong?