Hi everyone,
I'm not good with SYS/BIOS as well as DSP/BIOS. I have a basic question. I have C6678L board and as everybody know, this board can be use with OpenMP compiler by TI. The Hello World example, from the main() do not call the BIOS_start(). It start and end in the main function. I need to use this OpenMP capability
At the same time, I need to transfer a very large file from my PC through tftp, and from help through these forum, I've managed to do the transfer. It is done by task. It started by BIOS_start() in the main() function and then pass to another function to do the transfer.
My question is, is it possible, after performing the file transfer, I can get back to the main() function to use the OpenMP capability in the main()? If possible, can someone please show me how and what to do from the XGCONF of my configuration (.cfg file).
If it is also possible to use OpenMP in a task, can someone prove this to me?
Thanks guys,
Rizuan